MQTT Sparkplug API
Netilion MQTT Sparkplug API
Section titled “Netilion MQTT Sparkplug API”This document explains how external controllers, gateways, and edge devices can send data to Netilion using the Sparkplug protocol 3.0.
IMPORTANT To use the MQTT Sparkplug API, you must have a Netilion subscription that supports third‑party FieldEdge add‑ons. This capability is not included in a Netilion Connect subscription. Please contact your Netilion Sales Partner to clarify which Netilion subscription best fits your needs.
Cloud Endpoints
Section titled “Cloud Endpoints”Your device connects directly to the secure MQTT broker of Netilion.
Available environments:
- Global:
mqtt2.netilion.endress.com:8883 - India only:
in.mqtt2.netilion.endress.com:8883
All communication requires TLS encryption.
Security & Access
Section titled “Security & Access”To connect successfully, the following is required:
TLS Encryption
Section titled “TLS Encryption”Your device must trust the cloud’s TLS root certificate. Download it here: https://developer.netilion.endress.com/resources/certificates/
Netilion Data Model Setup
Section titled “Netilion Data Model Setup”To ensure that Sparkplug topics from connected external edge devices are accepted, the Netilion data model must be configured accordingly. This configuration consists of three key elements:
- Location Node – Represents the physical or logical location within the system hierarchy.
- Edge Device Object – Represents the actual physical edge device.
- Asset Objects – Each connected device must be represented by a corresponding asset object to ensure proper mapping and reliable data flow.
A FieldEdge Uplink AddOn must be assigned to the subscription.
Location Node
Section titled “Location Node”A location node object groups related objects within the Netilion data model. It is important that all connected devices (asset objects) are grouped under this node object. A hierarchical node structure below this location node is also possible.
Create the node in Netilion under All Objects. Set the node type to “Location” and assign it to the edge device object.
The Node ID is used as part of the Sparkplug topic structure.
Edge Device Object
Section titled “Edge Device Object”Create a 3rd‑party edge device on the Netilion Edge Device page and assign it to the corresponding location node. A free FieldEdge Uplink AddOn must be assigned to the subscription to create the edge device.
The generated Edge ID is used as part of the Sparkplug topic structure.
Asset Objects
Section titled “Asset Objects”Create for each device which you want to integrate a corressponding asset object.
The device’s serialnumber is applied as unique key and part of the Sparkplug topic structue.
Technical User Credentials
Section titled “Technical User Credentials”In Netilion in the properties of your corresponding edge device object you can create the credentials of the needed technical user.
ClientID
Section titled “ClientID”In MQTT, the ClientID is a unique identifier that every client must provide when connecting to an MQTT broker. For Netilion the ClientID must begin with the authenticated technical username. A suffix may be appended to distinguish multiple clients under the same account.
Valid Formats
Section titled “Valid Formats”<username><username>-<client-specific-identifier>
Data Model and Topic Structure
Section titled “Data Model and Topic Structure”Netilion uses the standard Sparkplug topic format:
spBv1.0/<Node ID>/<Message Type>/<Edge ID>/<device's serialnumber>Components:
- Node ID → The assigned node identifier
- Edge ID → The assigned edge device identifier
- Device Serialnumber → The connected instrument or controller. This must correspond to a Netilion asset.
Correct ID assignment ensures that all incoming data is routed to the right assets.
Supported Sparkplug Message Types
Section titled “Supported Sparkplug Message Types”| Message Type | Description | Supported |
|---|---|---|
| NBIRTH | Edge device announces it is online | yes |
| NDEATH | Edge device goes offline | yes |
| DBIRTH | Device announces all values it can send | yes |
| DDEATH | Device goes offline | yes |
| NDATA | Edge device live or historical data updates | partly |
| DDATA | Live or historical data updates | yes |
| NCMD | Cloud → Edge device control commands | no |
| DCMD | Cloud → device control commands | yes, optional |
| STATE | Sparkplug Host Applications to denote is online or not | no |
Edge Device Definition (NBIRTH)
Section titled “Edge Device Definition (NBIRTH)”When a edge device first connects, it sends a NBIRTH message.
Device Definition (DBIRTH)
Section titled “Device Definition (DBIRTH)”When a device first connects, it sends a DBIRTH message describing its available values.
Each DBIRTH message can include:
- Value names (e.g.
temperature,volumeflow,pump_on) - Data type (supported types Float, Integer, Boolean, etc.)
- Engineering unit (Netilion Unit Codes must be used: https://developer.netilion.endress.com/development/date_unit_currency/#units)
- Device Health State
- receive DCMD as Boolean (e.g.
desired_state) - send events as Boolean (e.g.
LocalEvent)
Example Payload:
{ "definition" : { "Properties/Device Health" : { "dataType" : "Int32" }, "VolumeFlow": { "dataType": "Float", "properties": { "UnitCode": { "type": "String", "value": "litre_per_hour" } } }, "desired_state": { "dataType": "Boolean" }, "Events/LocalEvent":{ "dataType": "Boolean" } }, "payload" : { "metrics" : [ { "name": "Properties/Device Health", "value": 0 }, { "name": "VolumeFlow", "value": 500 } ] }}Live and Historical Data (DDATA)
Section titled “Live and Historical Data (DDATA)”Devices can send:
- Live values
- Backfilled historical values (with device timestamps)
- Multiple values in one message (recommended for efficiency)
Example Payload with multiple values, with timestamps in one message:
{ "metrics": [ { "timestamp": "2025-07-01T01:24:34.991Z", "value": 6, "name": "ValueName", "isHistorical": true }, { "timestamp": "2025-07-02T02:23:12.992Z", "value": 7, "name": "ValueName", "isHistorical": true }, { "timestamp": "2025-07-03T03:23:12.993Z", "value": 8, "name": "ValueName", "isHistorical": true }, { "timestamp": "2025-07-04T04:23:12.994Z", "value": 9, "name": "ValueName", "isHistorical": true }, { "timestamp": "2025-07-05T05:23:12.995Z", "value": 10, "name": "ValueName", "isHistorical": true } ]}Netilion accepts:
- Timestamps: ISO 8601 or Unix epoch
- Value types: see chapter “Supported data types”
Device Health / Status Codes
Section titled “Device Health / Status Codes”Netilion maps Sparkplug health values to standardized status categories.
| Health Code | Netilion Interpretation |
|---|---|
| 0 | OK |
| 1 | Failure |
| 2 | Check Function |
| 3 | Out of Specification |
| 4 | Maintenance Required |
Status can be sent in DBIRTH or DDATA.
Events
Section titled “Events”Devices can report local events using Sparkplug values with the prefix:
Events/<EventName>Examples:
- Pump started
- Valve closed
- Local alarm
- Process step completed
Events appear directly in Netilion’s event logs
Example DDATA Payload:
{ "metrics": [ { "name": "Events/LocalEvent", "value": 1, } ]}Remote Commands “DCMD” (Optional)
Section titled “Remote Commands “DCMD” (Optional)”If enabled, the Netilion can send control commands to the device, such as:
- Switching equipment on/off
- Changing operating modes
- Triggering device actions
Topic structure:
spBv1.0/<Node ID>/DCMD/<Edge ID>/<device's serialnumber>Example DCMD Payload received from Netilion:
{ "metrics": [ "value": false, "type": "Boolean", "name": "desired_state", "timestamp": "2026-02-11T14:26:29.624Z" ]}Requirements:
- Ensure the proper use of a Netilion Application that supports remote commands, along with the correct configuration of the associated asset in accordance with the user guide for the specific Netilion Application
- The DBIRTH and DDATA Message must follow the user guide for the specific Netilion Application
WARNING Safety Considerations for DCMD Deployment. When deploying asset actions using DCMD on a customer site, it is essential to introduce it in a controlled, safe, and secure manner, particularly where field equipment can be influenced remotely via Sparkplug commands.
The following actions should support this:
- Define remote asset actions. Clearly document which asset actions can be triggered remotely and confirm device support for each action.
- Perform onsite risk assessment. Assess risks related to remote command execution during testing and define mitigation measures before activation.
- Review customer SOPs. Verify that remote operation complies with customer Standard Operating Procedures and required approvals.
- Verify controller safety behavior. Ensure installed controllers handle remote commands safely and do not bypass local safety mechanisms.
Supported data types
Section titled “Supported data types”The following data types are supported by the Netilion Sparkplug API Int8, Int16, Int32, Int64, UInt8, UInt16, UInt32, UInt64, Float, Double, Boolean
Rate Limits
Section titled “Rate Limits”To ensure platform stability:
| Limit | Value |
|---|---|
| Maximum Sparkplug messages per device per minute | 60 |
| Maximum payload size | 256 MB per message |